Report of the Statutory Auditor on the Consolidated Financial Statements

To the General Meeting of ABB Ltd, Zurich

As statutory auditor, we have audited the consolidated financial statements of ABB Ltd, which are comprised of the consolidated balance sheets as of December 31, 2014 and 2013, and the related consolidated statements of income, comprehensive income, cash flows and changes in stockholders’ equity, and notes thereto (pages 114–164), for each of the three years in the period ended December 31, 2014.

Board of Directors’ Responsibility

The Board of Directors is responsible for the preparation of these consolidated financial statements in accordance with U.S. generally accepted accounting principles and the requirements of Swiss law. This responsibility includes designing, implementing and maintaining an internal control system relevant to the preparation of consolidated financial statements that are free from material misstatement, whether due to fraud or error. The Board of Directors is further responsible for selecting and applying appropriate accounting policies and making accounting estimates that are reasonable in the circumstances.

Auditor’s Responsibility

Our responsibility is to express an opinion on these consolidated financial statements based on our audits. We conducted our audits in accordance with Swiss law, Swiss Auditing Standards and the standards of the Public Company Accounting Oversight Board (United States). Those standards require that we plan and perform the audit to obtain reasonable assurance whether the consolidated financial statements are free of material misstatement.

An audit involves performing procedures to obtain audit evidence about the amounts and disclosures in the consolidated financial statements. The procedures selected depend on the auditor’s judgment, including the assessment of the risks of material misstatement of the consolidated financial statements, whether due to fraud or error. In making those risk assessments, the auditor considers the internal control system relevant to the entity’s preparation of the consolidated financial statements in order to design audit procedures that are appropriate in the circumstances. An audit also includes evaluating the appropriateness of the accounting policies used and the reasonableness of accounting estimates made, as well as evaluating the overall presentation of the consolidated financial statements. We believe that the audit evidence we have obtained is sufficient and appropriate to provide a basis for our audit opinion.

Opinion

In our opinion, the consolidated financial statements referred to above present fairly, in all material respects, the consolidated financial position of ABB Ltd as of December 31, 2014 and 2013, and the consolidated results of its operations and its cash flows for each of the three years in the period ended December 31, 2014, in accordance with U.S generally accepted accounting principles and comply with Swiss law.

Report on other legal requirements

We confirm that we meet the legal requirements on licensing according to the Auditor Oversight Act (AOA) and independence (article 728 CO and article 11 AOA) and that there are no circumstances incompatible with our independence.

In accordance with article 728a paragraph 1 item 3 CO and Swiss Auditing Standard 890, we confirm that an internal control system exists, which has been designed for the preparation of consolidated financial statements according to the instructions of the Board of Directors.

We recommend that the consolidated financial statements submitted to you be approved.

We also have audited, in accordance with the standards of the Public Company Accounting Oversight Board (United States), ABB Ltd’s internal control over financial reporting as of December 31, 2014, based on criteria established in Internal Control – Integrated Framework issued by the Committee of Sponsoring Organizations of the Treadway Commission (2013 framework) (COSO), and our report dated March 5, 2015 expressed an unqualified opinion on the effectiveness of ABB Ltd’s internal control over financial reporting.

Ernst & Young AG

Leslie Clifford
Licensed audit expert
(Auditor in charge)

Robin Errico
Licensed audit expert

Zurich, Switzerland
March 5, 2015